Cabac’s S-click range of 2in1 timer on/off switches and soon to be released dimmer range was engineered and manufactured in South Australia through Cabac’s sister company Hendon Semi-Conductors.We need a technologically advanced timer and on/off switch and dimmer range which was suitable for the rapidly changing energy efficient lighting market in Australia” says Bradley Dowe CEO.

Hendon was ideally suited to develop such advanced technology as they have over 25 Electronic/Design Engineers while the manufacturing facility processes are certified for some of the most stringent quality production processes in the world such as medical, automotive and military.

 S-click-range-200x200x
Hendon was ideally suited to develop such advanced technology as they have over 25 Electronic/Design Engineers while the manufacturing facility processes are certified for some of the most stringent quality production processes in the world such as medical, automotive and military. “This is home grown engineering and manufacturing technology as we are proud to say MADE IN AUSTRALIA”, continues Bradley.

The switch range was designed from the ground up to be suitable for the Australian market conditions and to keep pace with the rapidly changing energy saving drive in the market. The range is suitable for most popular home and commercial applications from LED lighting, traditional lights, fans, bathroom heaters and extractors; pumps and garden features.

“ The list of suitable product applications is quite extensive and Electricians should refer to the in store selection chart to see if their particular light is suitable” says Bradley.The S-Click products are the first to have been designed with extremely low standby power for use with high efficiency low power LED lighting systems. The dimmer range features “Ripple Tone Rejection” – a patent pending combination of hardware and algorithmic firmware calculation technology which minimises lamp flicker when ripple tones come down the line.

They also have Over-voltage, Over-current and Over-temperature protection to suit Australian conditions.

Cabac’s S-Click Smart switch range of switches and soon to be released dimmers are suitable for the most popular range of lighting products and will also retrofit into the most popular existing light switch plates sold in Australia today.

 NEW-CABAC-logo_Byline153x45px

© 2018 Rexel Electrical  |  Legal  |  Rexel Australia  |  Rexel Global