An important milestone in the phasing out of inefficient lamps will be introduced in April 2012. The ruling addresses the maximum wattage for ELV halogen lamps above 37 watts in accordance with Australian Standard AS4934.2-2011 Part 2: Mimimum Energy Performance Standards (MEPS), which states “For ELV halogen reflector lamps, the average measured wattage shall be no more than 37W.
With the enforcement date being April 2012. The relevant section of AS4934.2-2011 will be legislated in each state and the expected outcome of the legislation is the 50 Watt MR16 halogen lamp will not be able to be imported after April 2012.

For more information please download the PDF