3M’s New 92-NBA Resin Joints Kits

Filed under: News,Products — Tags: , , , , — Frida @ 4:01 pm

3M have a new one-part mould body with innovative sealing system requiring no cutting to size or taping, new 3M 92-NBA series Resin Joints Kits offer unmatched speed of installation.

BUY NOW!

3M’s Closed Mix-Pour resin bags are now enhanced with a new integrated resin delivery system. Designed to eliminate almost any chance of skin contact and reduce vapour inhalation from the resin itself, this gives the user superb control over the resin mixing and pouring process – avoiding unnecessary spills and wastage.

Further, 3M’s high quality resin compounds, renowned for their durability and reliability, are redeveloped to fully comply with EU environmental and user safety regulation changes.

Contact #8 – Available Now

The August/September Edition of Contact Magazine is out now! Click on the image to open in our interactive page turner format.

As always, if you would like to receive a copy of our Contact Magazine delivered directly to your mailbox, simply register your details with us and check the ‘Contact Magazine’ selection.

PSA Lock Alarms

Filed under: News,Products — Tags: , , , , , — Frida @ 12:02 pm

The NEW Lock Alarm from PSA offers an extra benefit other than a standard lock, it also has a built in high decibel alarm that is set off when someone attempts to cut through the lock and steel your belongings.

Lock Alarms provide inexpensive protection for all household items and also ideal for contractors that are looking for that extra protection when storing tools and/or equipment either on the construction site, or in their vehicles.



The Maxi Lock

Features:
■ Ultra hard steel cable covered by a protective vinyl sleeve
– 12mm diameter
■ Flashing LED deters thieves
■ High security key and lock cylinder
■ 1.5m cable
■ Suitable for indoor and outdoor use
■ Requires 2 x ‘AAA’ batteries (not included)
■ Batteries fit inside a tamper proof compartment
■ Optional same key & lock for bulk purchase
■ Weight: 450g

The Regular Lock

Features:
■ Compact design – 14cm x 7.5cm x 5cm
■ Flashing LED deterrent
■ 2.4m cable
■ Cable stores neatly around lock unit when not in use
■ Suitable for indoor and outdoor use
■ Requires 1 x 9 volt battery (not included)
■ Battery fits inside a tamper proof compartment
■ Weight: 420g

Power Shortages and Blackouts Predicted

Filed under: Uncategorized — Tags: , , — Frida @ 10:43 am

As electricity demands rise, predictions have been made to the future of the electricity.  ABC News reports that there are some industry players that are warning consumers to be prepared for blackouts and power shortages.

BBY market analyst Mike Harrowell told ABC News that  the outlook is bleak.  ”We are likely to be running into a shortage of capacity sometime within the next five years,” he said TruEnergy’s Richard McIndoe sees a similar outlook. ”I think there’s going to be real challenges during the peak times,” he said. ”We are not seeing a great deal of investment … whether it’s a base load supply or peak supply now because of this uncertainty.”

However, although there are many people who believe there will be a problem as demand rises some believe that the industry will be able to cope as it has been for the last 10 years by planning ahead and investing.  ”There has been more than 10,000 megawatts of new generation in the market, which is between 20 and 25 per cent of the total existing capacity so that’s a pretty high replacement rate,”  said Carl McCamish, of Origin Energy to ABC News.

“You’d say that that’s quite a lot of investment for a market of our size over that period of time and right up even through today you’ve got a lot of investment going on in wind and the solar and you are seeing investment in the PICA plants.

“It’s not a question of power shortages. Power shortages only happen if you’ve got not enough capacity in the system. In the PICA plants, the smaller plants that can ramp up and down quickly at times of peak demand – they’re the ones, as I say, that we’ve been investing in and the market is projecting to invest in as well. They will cover the issue of the lights going off.”